earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Server, Software Administrator
Functionalities: Engineering
Product version: 1.8, 1.9
6/25/2015

Starting the Enterprise Server Windows Service

You start the server manually in case you previously have stopped it.

Important:

Ensure that you have a working and available license. A working license is required to start the server. For more information, see Licenses .

Note:
  • An Enterprise Server is automatically started when installed and when Windows is started.

Show More
action_close

​The Software Administrator installs with the Enterprise Server installation package. You use the Software Administrator to start and stop the server service and configure the ports of the Enterprise Server.

Other server settings, for example e-mail service, time, and time zone settings are configured through WorkStation.

Service

The Enterprise Server runs in the background as a Windows service. You start and stop the server service through the Software Administrator or Windows Service. Before shutting down the server, make sure the stop does not negatively affect your site.

Ports

The Enterprise Server uses HTTP and TCP protocols to communicate with other servers and clients. In the Software Administrator, you configure the port number of each protocol the server listens to when communicating through a specific protocol.

To configure a protocol port number, you first have to stop the running Enterprise Server service.

Note:

Port changes you have made using Software Administrator are not automatically updated in the Communication view for SmartStruxure servers.

Database Location

In the Software Administrator, you find the path to the location where the Enterprise Server writes and stores data and objects that are created by either the Enterprise Server or the user.

Enterprise Server System Log

The Enterprise Server System log contains events logged by the Enterprise Server. Examples of logged events are start up sequence, port settings, failures, run time, and current server status.

To start the Enterprise Server Windows service
  1. In the Software Administrator , click the tab of the Enterprise Server .

  2. Click Start Service .

     
    action_zoom_plus_stroke
  • Stopping the Enterprise Server Windows Service
  • Software Administrator
  • Software Administrator – Enterprise Server View
  • Starting Software Administrator
  • Licenses
  • ​Enterprise Server does not Start