You add an exception event to configure an exception that is to apply instead of a scheduled weekly event for a single date, date range, or a time pair.
You cannot add, edit, or delete schedule events in a Xenta Schedule when a Xenta Central schedule has been assigned to it.
The number of events a Xenta Central schedule can have is determined by the Menta application.
An added exception event overrides any weekly events for all of the selected days.
In WebStation, in the System Tree pane, select the schedule to which you want to add the exception event.
In the Xenta Schedule editor, click
Click
Click
In the Span column, select Interval , On all day or Off all day .
If you select Interval in the Span column, enter the start time and end time for the interval.
Select the weekdays the exception event is to be in service.
Click Save .