Productos WebStation
Funcionalidades: Programaciones
Versión del producto: 1.8
10/06/2016

Adding an Exception Event to a Xenta Schedule in WebStation

You add an exception event to configure an exception that is to apply instead of a scheduled weekly event for a single date, date range, or a time pair.

Mostrar más
action_close

Xenta Time Schedules and Xenta Central Time Schedules can be edited in WebStation. You can add, edit and delete weekly and exception events. You can assign and unassign lead Xenta central schedules. The Xenta Time Schedules and Xenta Central Time Schedules must be created using WorkStation.

Para obtener más información, consulte Cómo funcionan las programaciones .

Xenta Central schedules are used to group Xenta 280/300/401 LonWorks device schedules created in the TSCH block in Menta Editor. When you use a Central schedule, you can change settings on whole Xenta schedule groups from a central place.

Para obtener más información, consulte Xenta Central Schedules .

Aviso

You cannot add, edit, or delete schedule events in a Xenta Schedule when a Xenta Central schedule has been assigned to it.

The number of events a Xenta Central schedule can have is determined by the Menta application.

Aviso

An added exception event overrides any weekly events for all of the selected days.

To add an exception event to a Xenta Schedule in WebStation
  1. In WebStation, in the System Tree pane, select the schedule to which you want to add the exception event.

  2. In the Xenta Schedule editor, click

     
    action_zoom_plus_stroke
    .

  3. Click

     
    action_zoom_plus_stroke
    to select Any year as start date or select a specific date to start the exception.

     
    action_zoom_plus_stroke
  4. Click

     
    action_zoom_plus_stroke
    to select Any year as end date or select a specific date as end date.

  5. In the Span column, select Interval , On all day or Off all day .

  6. If you select Interval in the Span column, enter the start time and end time for the interval.

  7. Select the weekdays the exception event is to be in service.

  8. Click Save .

  • Xenta Schedules in WebStation
  • Editing or Deleting a Weekly Event in a Xenta Schedule in WebStation