earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: WebStation
功能: 时间表
产品版本: 1.8
2016/6/10

Editing or Deleting an Exception Event in a Xenta Schedule in WebStation

You edit an exception event to change the time range, start and stop date, start and stop time, or weekdays of an exception event.

显示更多
action_close

Xenta Time Schedules and Xenta Central Time Schedules can be edited in WebStation. You can add, edit and delete weekly and exception events. You can assign and unassign lead Xenta central schedules. The Xenta Time Schedules and Xenta Central Time Schedules must be created using WorkStation.

有关更多信息,请参阅 时间表运作方式 .

Xenta Central schedules are used to group Xenta 280/300/401 LonWorks device schedules created in the TSCH block in Menta Editor. When you use a Central schedule, you can change settings on whole Xenta schedule groups from a central place.

有关更多信息,请参阅 Xenta Central Schedules .

重要:

You cannot add, edit, or delete schedule events in a Xenta Schedule when a Xenta Central schedule has been assigned to it.

The number of events a Xenta Central schedule can have is determined by the Menta application.

To edit or delete an exception event in a Xenta schedule in WebStation
  1. In WebStation, in the System Tree pane, select the schedule containing the exception event you want to edit.

  2. In the Xenta Schedule editor, click

     
    action_zoom_plus_stroke
    .

  3. Click

     
    action_zoom_plus_stroke
    to select Any year as start date or select a specific date to start the exception.

     
    action_zoom_plus_stroke
  4. Click

     
    action_zoom_plus_stroke
    to select Any year as end date or select a specific date as end date.

  5. In the Span column, select Interval , On all day or Off all day .

  6. If you select Interval in the Span column, enter the start date and end date for the interval.

  7. Select the weekdays the exception event is to be in service.

  8. Click Save .

To delete an exception event, click the trash can.

  • Xenta Schedules in WebStation
  • Adding an Exception Event to a Xenta Schedule in WebStation