earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WorkStation
Functionalities: Basic Functionality
Product version: 1.9
12/14/2016

Status Bar

Use the Status bar to view information on the following items:

  • connectivity status

  • security certificates

  • which SmartStruxure server the user is logged on to

  • the name of the logged on user account

  • which domain the user is logged on to

  • the current language

  • the measurement system

 
action_zoom_plus_stroke Status bar
Figure: Status bar

Component

Description

 
action_zoom_plus_stroke

Indicates that the security certificate is valid.

 
action_zoom_plus_stroke

Indicates that the security certificate cannot be validated.

 
action_zoom_plus_stroke

Connected to

Indicates that WorkStation is connected to the SmartStruxure server.

 
action_zoom_plus_stroke

Trying to connect to

Indicates that WorkStation is disconnected from the SmartStruxure server and trying to connect.

User account

Displays the account you are currently using.

Domain

Displays the domain you are logged on to.

Current language

Displays the current display language of the system

Measurement system

Displays the selected measurement system for the system

  • Workspaces
  • WorkStation Workspace