Backup is the process of copying and storing data so that the copy can be used to restore data if a loss occurs. You can also use a backup to revert to an older version. In the EcoStruxure BMS, you can perform backups on an all EcoStruxure BMS servers and their devices. EcoStruxure BMS server backups should take place during non-business hours.
Using WorkStation, you can back up data to the local drive of each installed EcoStruxure BMS server. The EcoStruxure Building Operation software stores the files by date in a predefined directory location on the server to which WorkStation is connected. Pour plus d'informations, voir Backup Sets .
The EcoStruxure Building Operation backup function enables you to back up different types of data.
Pour plus d'informations, voir Types of Data .
Backup sets are compressed backup files used for restoring data. The EcoStruxure Building Operation software stores the local backup set for an Enterprise Server or field servers in the Local folder within the Backup sets folder.
Pour plus d'informations, voir Backup Sets .
A scheduled backup is an automated way to back up data on an EcoStruxure BMS server. You can back up EcoStruxure BMS servers individually using each EcoStruxure BMS server’s local backup rule. You can also use backup rules to synchronize the backups of all the EcoStruxure BMS servers on your network.
Pour plus d'informations, voir Scheduled Backups .
Manual Backup is a non-automated process of copying and storing data on a selected EcoStruxure BMS server. You can use this option to create backups on an as-needed basis. You can also manually restore the data at any time.
Pour plus d'informations, voir Manual Backups .
Mass backup is a method of performing a manual, simultaneous backup of all the EcoStruxure BMS servers in the network, which is useful for capturing data at a critical point, such as prior to an upgrade. You can choose which EcoStruxure BMS servers you want to back up along with the type of data for each.
Pour plus d'informations, voir Mass Backup .
Before upgrading the system, it is strongly recommended that you archive the historical data and back up the EcoStruxure BMS servers to preserve the current data and configurations.
Pour plus d'informations, voir System Backup .
Backup Status displays the statuses of an EcoStruxure BMS server: Ready, Backing up, or Backup succeeded.
Pour plus d'informations, voir Backup Status .