earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: Device Administrator, Enterprise Central, Enterprise Server, Function Block Editor, Graphics Editor, ​License Administrator, ​License Server, Script Editor, Software Administrator
功能: 基本功能
产品版本: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018/5/18

Reinstallation

This is an additional solution instead of first manually uninstalling the current product and then installing a new copy.

通知

数据丢失

Back up the Enterprise Server before reinstalling the product. ​All​ user settings, database information, and system files related to this product are erased and replaced. 有关更多信息,请参阅 Backing Up EcoStruxure BMS Servers Manually .

不遵照这些说明可导致数据丢失。

To replace your current version, you start with the installation package of the product you want to reinstall. If the installation package recognizes an earlier installation of the EcoStruxure Building Operation product within the same major and minor version number but lower maintenance number, the installation wizard asks if you want to uninstall the current version before installing this package. 

注释:

Before reinstalling a License Server or Enterprise Server, you must stop related Windows services.

  • Backing Up EcoStruxure BMS Servers Manually
  • Reinstalling the Device Administrator Installation
  • Reinstalling the Enterprise Server
  • Reinstalling the License Administrator and the License Server
  • Reinstalling WorkStation and Client Tools
  • Installation Overview