earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2024, 7.0
2024/12/2

Styling the Alarm States in the Alarms Pane and Alarm Views

You style the appearance of the different alarm states in the Alarms pane and Alarm Views to easily separate the alarm states from each other.

显示更多
action_close

You use the Alarms pane and the Alarm View to view and administer alarms. When an alarm is triggered, it is displayed in the Alarms pane or Alarm Views together with information about the alarm. You can edit the Alarm View filter to display the Alarm View only when certain alarms are triggered. You can create and use more than one Alarm View. The Alarms pane and each Alarm View can be customized with an alarm filter to show information that is relevant to the user who supervises the alarms. Customized settings are lost when you perform a system upgrade.

In the Alarms pane and Alarm Views, you can also open a detailed view to inspect all properties for a selected alarm.

 
action_zoom_plus_stroke The Alarms pane
图: The Alarms pane

Through Control Panel, you can customize the appearance of different alarm states that are displayed in the Alarms pane and Alarm Views. For example, you can change the font style, font size, background color, and font color.

You can also configure the alarm to flash or play a sound when it is triggered.

Alarm View standard filter and layout

A standard layout defines the columns that are included in the Alarms pane, Events pane, Alarm View, or Event View, the order in which they are displayed, whether or not the alarms or events are grouped in any way and whether they are displayed in an ascending or descending order. A standard filter defines the conditions that have to be met before the alarms or events are displayed in the pane or a View. The standard layout and filter is saved for the pane or View to which you made the changes. The standard layout and filter is displayed for all users of the the EcoStruxure BMS.

有关更多信息,请参阅 Alarm View and Event View Standard Filter and Layout .

To style the alarm states in the Alarms pane and Alarm Views
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Styling .

  4. In the Alarm Styles view, double-click the alarm state you want to style.

  5. In the Font box, click the Browse button.

  6. In the Font dialog box, select the font, font style, and font size that you want to use in the Alarms pane and Alarm Views.

  7. Click OK .

  8. In the Background color box, click the Browse button.

  9. In the Color dialog box, select the color for the background of the alarm state row.

  10. Click OK .

  11. In the Font color box , click the Browse button.

  12. Select the color for the font of the alarm state text.

  13. Click OK .

  14. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Creating a Filtered Alarm View
  • Acknowledged Style Properties
  • Alarm Style Properties
  • Disabled Style Properties
  • Fault Style Properties
  • Reset Style Properties
  • Alarms Pane and Alarm View Customization
  • Changing the Alarm State Sort Order