earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 2024, 7.0
12/3/2024

Create Sum Alarm Wizard – Alarm Trigger Page

Use the Alarm Trigger page to configure the trigger settings of the sum alarm.

 
action_zoom_plus_stroke Sum Alarm trigger page
Figure: Sum Alarm trigger page

Table: Sum Alarm Trigger Page

Component

Description

 
action_zoom_plus_stroke

Add condition

Select the alarm filter conditions for the alarms you want to include.

For more information, see Alarm Filters .

You can use wildcards when setting up filter conditions. For more information, see Filter Condition Wildcards .

 
action_zoom_plus_stroke

Remove condition

Remove the alarm filter conditions for the alarms you want exclude.

 
action_zoom_plus_stroke

Add row

Click to add an additional row with the same condition.

 
action_zoom_plus_stroke

Remove row

Click to remove a condition row.

 
action_zoom_plus_stroke

Clear all

Click to clear the selected conditions.

Alarm State

Displays the alarm state of the alarm. For more information, see Alarm States .

Matching alarms count

Displays the number of alarms that currently meet the criteria of the sum alarm.

Disable alarm

Select to disable the alarm, for example, before deployment.

Alarm delay

​Enter the time, in seconds, the alarm has to be within the alarm criteria before the alarm is triggered.

Reset delay

​Enter the time, in seconds, the alarm has to be within the reset criteria before the alarm state is changed from alarm to reset.

Shunt variable 1

​Enter the shunt variable that is used to enable or disable the alarm. For more information, see Shunt Variables .

Invert

Select to invert the shunt value, that is, enable the alarm when the shunt value is active and disable the alarm when the shunt value is inactive. For more information, see Shunt Variables .

Operator

Select AND or OR to add logic between the first and the second shunt variable. For more information, see Shunt Variables .

Shunt variable 2

​Enter the second shunt variable that is used to enable or disable the alarm. For more information, see Shunt Variables .

Invert

Select to invert the shunt value, that is, enable the alarm when the shunt value is active and disable the alarm when the shunt value is inactive. For more information, see Shunt Variables .

  • Sum Alarms
  • Sum Alarm Properties – Basic Tab
  • Alarm Filters
  • Filter Condition Wildcards
  • Create Alarm Wizard – Presentation Page
  • Create Alarm Wizard – User Action Page
  • Create Alarm Wizard – Attachment Page
  • Create Object Dialog – Naming the Object Page