earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2.0, 2.1, 3.0, 3.1
2018/12/18

Create Sum Alarm Wizard – Alarm Trigger Page

Use the Alarm Trigger page to configure the trigger settings of the sum alarm.

 
action_zoom_plus_stroke Sum Alarm trigger page
图: Sum Alarm trigger page

表格: Sum Alarm Trigger Page

Component

Description

 
action_zoom_plus_stroke

Add condition

Select the alarm filter conditions for the alarms you want to include.

有关更多信息,请参阅 Alarm Filters .

You can use wildcards when setting up filter conditions. 有关更多信息,请参阅 Filter Condition Wildcards .

 
action_zoom_plus_stroke

Remove condition

Remove the alarm filter conditions for the alarms you want exclude.

 
action_zoom_plus_stroke

Add row

Click to add an additional row with the same condition.

 
action_zoom_plus_stroke

Remove row

Click to remove a condition row.

 
action_zoom_plus_stroke

Clear all

Click to clear the selected conditions.

Alarm State

Displays the alarm state of the alarm. 有关更多信息,请参阅 Alarm States .

Matching alarms count

Displays the number of alarms that currently meet the criteria of the sum alarm.

Disable alarm

Select to disable the alarm, for example, before deployment.

Alarm delay

​Enter the time, in seconds, the alarm has to be within the alarm criteria before the alarm is triggered.

Reset delay

​Enter the time, in seconds, the alarm has to be within the reset criteria before the alarm state is changed from alarm to reset.

Shunt variable 1

​Enter the shunt variable that is used to enable or disable the alarm. 有关更多信息,请参阅 Shunt Variables .

Invert

Select to invert the shunt value, that is, enable the alarm when the shunt value is active and disable the alarm when the shunt value is inactive. 有关更多信息,请参阅 Shunt Variables .

Operator

Select AND or OR to add logic between the first and the second shunt variable. 有关更多信息,请参阅 Shunt Variables .

Shunt variable 2

​Enter the second shunt variable that is used to enable or disable the alarm. 有关更多信息,请参阅 Shunt Variables .

Invert

Select to invert the shunt value, that is, enable the alarm when the shunt value is active and disable the alarm when the shunt value is inactive. 有关更多信息,请参阅 Shunt Variables .

  • Sum Alarms
  • Sum Alarm Properties – Basic Tab
  • Alarm Filters
  • Filter Condition Wildcards
  • Create Alarm Wizard – Presentation Page
  • Create Alarm Wizard – User Action Page
  • Create Alarm Wizard – Attachment Page
  • Create Object Wizard – Naming the Object Page