earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Server, Virtual Project Servers
Functionalities: Localization
Product version: 1.8
10/13/2016

Synchronize Network Time Settings

​You can establish a lead and shadow relationship to synchronize the time on all your SmartStruxure server devices with the same network time server. The Date and Time object on the lead server contains the network time server addresses that are inherited by shadow servers.

 
action_zoom_plus_stroke The Date and Time object is found in the server System, Time Settings folder.
Figure: The Date and Time object is found in the server System, Time Settings folder.

The date and time lead object is configured through the Control Panel - Network time and time zones on the Enterprise Server.​

The Network time synchronization on shadow Automation Servers option on the Enterprise Server contains the addresses that are inherited by all shadow SmartStruxure server devices. If you disable this option, established shadow and lead relationships consist but the shadow SmartStruxure server devices do not synchronize their network time server addresses with the lead Enterprise Server. Instead, the SmartStruxure server devices use their own time settings.

Note:
  • The addresses in the Automation Server - Date & Time do not affect the Enterprise Server time and date settings. For more information, see Network Time .

  • Lead and Shadow Relationship
  • Network Time
  • Enterprise Server – Date & Time View
  • Synchronizing Time Settings on Multiple SmartStruxure Server Devices