earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 本地化
产品版本: 2.0, 2.1, 3.0, 3.1
2018/8/22

Synchronize Network Time Settings

​You can establish a lead and shadow relationship to synchronize the time on all your EcoStruxure BMS servers with the same network time server. The Date and Time object on the lead server contains the network time server addresses that are inherited by shadow servers.

The Network time synchronization on shadow Automation Servers option on the Enterprise Server contains the addresses that are inherited by all shadow SmartX servers. If you disable this option, established shadow and lead relationships consist but the shadow SmartX servers do not synchronize their network time server addresses with the lead Enterprise Server. Instead, the SmartX servers use their own time settings.

注释:
  • The addresses in the Automation Server - Date & Time do not affect the Enterprise Server time and date settings. 有关更多信息,请参阅 Network Time .

  • Lead and Shadow Relationship
  • Network Time
  • Date & Time View
  • Synchronizing Time Settings on Multiple SmartX Servers