earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 2024, 7.0
12/2/2024

Synchronized Backups

A synchronized backup is a method of performing a recurring, simultaneous backup of a selected number of EcoStruxure BMS servers. You can use a lead and shadow relationship to automate all the EcoStruxure BMS server backups on your network. Using this method, you configure and manage one lead backup rule on one EcoStruxure BMS server, which other backup rules can reference.

 
action_zoom_plus_stroke Synchronized recurring backup – Lead/Shadow method
Figure: Synchronized recurring backup – Lead/Shadow method

The system synchronizes all the shadow rules with the lead backup rule, and all the shadow schedules with the lead schedule. For more information, see Synchronizing EcoStruxure BMS Server Backups on a Network .

  • Backup Rules View