earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Localization
Product version: 3.2
10/15/2020

Synchronizing Time Zone Settings on Multiple SmartX Servers

You define the time zone settings for connected shadow SmartX servers by changing the lead Enterprise Server time zone settings.

Show More
action_close

​​You can establish a lead and shadow relationship to synchronize the time zone settings on all your EcoStruxure BMS servers. The Time Zone object on the lead server contains the time zone settings that are inherited by shadow servers.

This is done automaticallly when you create a new server. For more information, see Creating a SmartX Server .

To synchronize the time zone settings on multiple SmartX servers
  1. In WorkStation, in the Search box, type “Time Zone” to search for the time zone object on all connected SmartX servers in your EcoStruxure BMS.

  2. Click the Search button

     
    action_zoom_plus_stroke
    .

  3. In the Search view, select the SmartX servers with the time zone you want to synchronize with the Enterprise Server time zone settings.

  4. Click the Show/Hide Property Grid button

     
    action_zoom_plus_stroke
    .

  5. Click the Zone Info tab.

  6. ​​In the Lead object box, enter /[Enterprise Server Name]/System/Time Settings/Time Zone .

  7. On the File menu, click Save .

  • Changing the Time Zone of an EcoStruxure BMS Server
  • Search Overview
  • Creating a Custom Time Zone of an EcoStruxure BMS Server
  • Synchronize Time Zone Settings
  • Lead and Shadow Relationship
  • Time Zone Properties – Basic Tab