earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Explicación de procesos

Explicación de procesos


Productos AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Localización
Versión del producto: 1.9
14/12/2016

Synchronizing Time Zone Settings on Multiple SmartStruxure Server Devices

You define the time zone settings for connected shadow SmartStruxure server devices by changing the lead Enterprise Server time zone settings.

Mostrar más
action_close

​​You can establish a lead and shadow relationship to synchronize the time zone settings on all your SmartStruxure servers. The Time Zone object on the lead server contains the time zone settings that are inherited by shadow servers.

 
action_zoom_plus_stroke Time Xone object on an Enterprise Server
Figura: Time Xone object on an Enterprise Server

The time zone lead object is configured through the Control Panel - Network time and time zone , on the Enterprise Server.

To synchronize the time zone settings on multiple SmartStruxure server devices
  1. In WorkStation, in the Search box, type “Time Zone” to search for the time zone object on all connected SmartStruxure server devices in your SmartStruxure solution system.

  2. Click the Search button

     
    action_zoom_plus_stroke
    .

  3. In the Search view, select the SmartStruxure server devices with the time zone you want to synchronize with the Enterprise Server time zone settings.

     
    action_zoom_plus_stroke
  4. Click the Show/Hide Property Grid button

     
    action_zoom_plus_stroke
    .

  5. Click the Zone Info tab.

     
    action_zoom_plus_stroke
  6. ​​In the Lead object box, enter /[Enterprise Server Name]/System/Time Settings/Time Zone .

  7. On the File menu, click Save .

  • Changing the Time Zone of a SmartStruxure Server
  • Search Overview
  • Creating a Custom Time Zone of a SmartStruxure Server
  • Synchronize Time Zone Settings
  • Lead and Shadow Relationship
  • Time Zone Properties – Basic Tab