earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Server, AS-P, Project Configuration Tool
功能: 本地化
产品版本: 2023
2024/11/29

Synchronizing Time Zone Settings on Multiple Automation Servers

You define the time zone settings for connected shadow automation servers by changing the lead Enterprise Server time zone settings.

显示更多
action_close

​​You can establish a lead and shadow relationship to synchronize the time zone settings on all your EcoStruxure BMS servers. The Time Zone object on the lead server contains the time zone settings that are inherited by shadow servers.

This is done automaticallly when you create a new server. 有关更多信息,请参阅 Creating an Automation Server .

To synchronize the time zone settings on multiple Automation servers
  1. In WorkStation, in the Search box, type “Time Zone” to search for the time zone object on all connected automation servers in your EcoStruxure BMS.

  2. Click the Search button

     
    action_zoom_plus_stroke
    .

  3. In the Search view, select the automation servers with the time zone you want to synchronize with the Enterprise Server time zone settings.

  4. Click the Show/Hide Property Grid button

     
    action_zoom_plus_stroke
    .

  5. Click the Zone Info tab.

  6. ​​In the Lead object box, enter /[Enterprise Server Name]/System/Time Settings/Time Zone .

  7. On the File menu, click Save .

  • Changing an EcoStruxure BMS Server Time Zone
  • Search Overview
  • Creating an EcoStruxure BMS Server Custom Time Zone
  • Time Zone Settings Synchronization
  • Lead and Shadow Relationship
  • Time Zone Properties – Basic Tab