earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos AS-B, AS-P, Project Configuration Tool
Funcionalidades: Localización
Versión del producto: 3.2
23/11/2020

Time and Time Zone Configuration in SmartX Server

​To adjust the SmartX server time, time zone, and DST, you have to access the SmartX server through a WorkStation.

When adjusting the server clock, you can either set the time manually or you can refer to a network time server that automatically synchronizes the clock. Manual adjusting is used when you configure or commission a SmartX server. When the SmartX server is running on a fully commissioned site, it is important that you use a network time server to avoid drifting time in the SmartX server.

Beside predefined time zones, you can also customize the SmartX server time zone settings.

When adjusting the SmartX server time through WorkStation, it is the SmartX server operating system clock you adjust. The EcoStruxure Building Operation software has a transparent layer above the SmartX server operating system which manages the information about the time zone and DST time offset.

 
action_zoom_plus_stroke  The SmartX Server uses the operating system clock to which the EcoStruxure Building Operation software adds the time zone offset and DST
Figura: The SmartX Server uses the operating system clock to which the EcoStruxure Building Operation software adds the time zone offset and DST

Instead of configuring the time of each SmartX server, you can create a lead and shadow relationship that makes it possible to configure several SmartX servers through a single Enterprise Server.

  • Lead and Shadow Relationship
  • Synchronize Network Time Settings
  • Synchronize Time Zone Settings
  • Time and Time Zone
  • Regional and Language Overview
  • SmartX Server – Date & Time View
  • Manually Changing the SmartX Server Time and Date
  • Synchronizing the SmartX Server Clock
  • Changing the Time Zone of an EcoStruxure BMS Server