earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: Enterprise Server, Project Configuration Server, Project Configuration Tool
功能: 本地化
产品版本: 1.8
2016/10/13

Time and Time Zone Configuration in Enterprise Server

​The Enterprise Server time and date settings are configured through the operating system settings on which the Enterprise Server is installed. The time zone offset, configured through the Enterprise Server, is added by Building Operation to the UTC time. The Enterprise Server time zone settings are therefore independent of the operating system time zone settings.

 
action_zoom_plus_stroke  The Enterprise Server uses the operating system clock on which the server is installed. Time zone offset and DST are then added by Building Operation to the UTC time.
图: The Enterprise Server uses the operating system clock on which the server is installed. Time zone offset and DST are then added by Building Operation to the UTC time.

To adjust your operating system clock, refer to your manufacturer’s manual for the operating system. The Enterprise Server time zone is configured on the Enterprise Server through WorkStation

注释:
  • Synchronize Network Time Settings
  • Synchronize Time Zone Settings
  • Time and Time Zone
  • Regional and Language Overview
  • Enterprise Server – Date & Time View
  • Creating a Custom Time Zone of a SmartStruxure Server
  • Configuring Regional Settings