When you create a schedule, the time zone of the SmartStruxure server that contains the schedule determines the execution of the events. If the schedule is copied to a SmartStruxure server in a different time zone, the specified dates and times relate to the new time zone.
For example, a schedule with an event defined to start at 08:00 Eastern Standard Time in a device located in Boston is copied to a device in London. The event would start at 08:00 Greenwich Mean Time.
When working within a schedule, you can display two different time zones. Building Operation also displays the time differential for the second time zone. For example, if you are working in Eastern Standard Time, the Greenwich Mean Time shows a +5 time differential.