earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Koncept

Koncept


Produkter: AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funktionaliteter: Tidsscheman
Produktversion: 3.2, 3.3, 2022
2020-10-15

Time Zones

When you create a schedule, the time zone of the EcoStruxure BMS server that contains the schedule determines the execution of the events. If the schedule is copied to an EcoStruxure BMS server in a different time zone, the specified dates and times relate to the new time zone.

For example, a schedule with an event defined to start at 08:00 Eastern Standard Time in a device located in Boston is copied to a device in London. The event would start at 08:00 Greenwich Mean Time.

When working within a schedule, you can display two different time zones. The schedule editor also displays the time differential for the second time zone. For example, if you are working in Eastern Standard Time, the Greenwich Mean Time shows a +5 time differential.

  • Schedules Overview
  • Schedule Events
  • Time and Time Zone