Use the Tools menu to open Control Panel or make a number of user settings.
Command |
Description |
Control Panel |
Click to open the Control Panel where you get access to some of the most used administration functions in Building Operation, such as alarms, domains, user accounts, backup and archiving, and engineering. 有关更多信息,请参阅 Control Panel View . |
Language |
Click to open the Language submenu where you select a different WorkStation language. 有关更多信息,请参阅 Language Packages . |
Measurement system |
Click to open the Measurement system submenu where you select a different local measurement system. 有关更多信息,请参阅 Units . |
Options |
Click to open the Options dialog box where you manage some local user settings. 有关更多信息,请参阅 Options Dialog Box . |