earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 基本功能
产品版本: 2.0, 2.1, 3.0, 3.1
2018/11/6

Tools Menu

Use the Tools menu to open Control Panel or make a number of user settings.

 
action_zoom_plus_stroke Tools menu
图: Tools menu

表格: Tools Menu

Command

Description

Control Panel

​​Click to open the Control Panel where you get access to some of the most used administration functions, such as alarms, domains, user accounts, backup and archiving, and engineering. 有关更多信息,请参阅 Control Panel Tab .

Language

Click to open the Language submenu where you select a different WorkStation language. 有关更多信息,请参阅 Language Packages .

Measurement system

Click to open the Measurement system submenu where you select a different local measurement system. 有关更多信息,请参阅 Units .

Database mode

Click to configure WorkStation to run in database mode so changes are saved to the EcoStruxure BMS server database and not sent to any physical devices. 有关更多信息,请参阅 Database Mode .

Options

Click to open the Options dialog box where you manage some local user settings.

  • Control Panel Tab
  • Language Packages
  • Units
  • Database Mode