earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos WebReports
Funcionalidades: Informes
Versión del producto: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
16/12/2021

Top Alarms Report

The Top Alarms report provides information about the most frequently occurring alarms for all EcoStruxure BMS servers. The EcoStruxure BMS server where the alarm originated and the monitored variable are included in the report. You can use the report to identify the number of times an alarm has been triggered and then determine the most problematic areas in your buildings. The percentage of the total number of alarms is also calculated.

The following table shows the input parameters for the report.

Tabla: Top Alarms Input Parameters

Input Parameters

Description

Start report date/time

Specifies the start date and time of the triggered alarms.

End report date/time

Specifies the end date and time of the triggered alarms.

Date filter

Specifies the date range of an operation, such as an alarm trigger, the running of a report schedule, or a read by the Reporting Agent.

For example, if you select Last 7 days for an alarm report, the report displays information about all alarms that were triggered during the last 7 days. If you select Last 7 days for the Report schedule report, the report displays information about all Report schedules that were run during the last 7 days. If you select Last 7 days for the Reporting Agent report, the report displays information about all Reporting Agent reads that occurred during the last 7 days.

Select Fixed date if you entered a Start report date/time and an End report date/time .

Show top

Specifies a number used to filter the top most frequently occurring alarms.

  • Factory Supplied Reports
  • Production Reports
  • WebReports Submit Form Page