earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Conceito

Conceito


Produtos: WebReports
Funcionalidades: Relatórios
Versão do produto: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
16-12-2021

Top System Alarms Per Server Report

The Top System Alarms Per Server report provides information about the most frequently occurring system alarms for a particular EcoStruxure BMS server. The report can be used by System Managers to identify and troubleshoot problems with a specified EcoStruxure BMS server.

The following table shows the input parameters for the report.

Tabela: Top System Alarms Per Server Input Parameters

Input Parameters

Description

Start report date/time

Specifies the start date and time of the triggered alarms.

End report date/time

Specifies the end date and time of the triggered alarms.

Date range filter

Specifies the date range of an operation, such as an alarm trigger, the running of a report schedule, or a read by the Reporting Agent.

For example, if you select Last 7 days for an alarm report, the report displays information about all alarms that were triggered during the last 7 days. If you select Last 7 days for the Report schedule report, the report displays information about all Report schedules that were run during the last 7 days. If you select Last 7 days for the Reporting Agent report, the report displays information about all Reporting Agent reads that occurred during the last 7 days.

Select Fixed date if you entered a Start report date/time and an End report date/time .

Server

Specifies the EcoStruxure BMS server that you want to audit.

Report view

Specifies the format, such as a table, for displaying the report.

Show top

Specifies a number used to filter the top most frequently occurring system alarms.

  • Factory Supplied Reports
  • Production Reports
  • WebReports Submit Form Page