earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: WebReports
功能: 报告
产品版本: 1.8, 1.9
2015/5/28

Top System Alarms Report

The Top System Alarms report provides information about the most frequently occurring system alarms for all SmartStruxure servers in your system. The report can be used by System Managers to identify and troubleshoot issues and problems with all SmartStruxure servers.

The following table shows the input parameters for the report.

表格: Top System Alarms Input Parameters

Input Parameters

Description

Start report date/time

Specifies the start date and time of the triggered alarms.

End report date/time

Specifies the end date and time of the triggered alarms.

Date filter

Specifies the date range of an operation, such as an alarm trigger, the running of a report schedule, or a read by the Reporting Agent.

For example, if you select Last 7 days for an alarm report, the report displays information about all alarms that were triggered during the last 7 days. If you select Last 7 days for the Report schedule report, the report displays information about all Report schedules that were run during the last 7 days. If you select Last 7 days for the Reporting Agent report, the report displays information about all Reporting Agent reads that occurred during the last 7 days.

Select Fixed date if you entered a Start report date/time and an End report date/time .

Show top

Specifies a number used to filter the top most frequently occurring system alarms.

  • Factory Supplied Reports
  • Production Reports
  • WebReports Submit Form Page