earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
功能: 趋势
产品版本: 2024, 7.0
2024/12/2

Trend Chart Axes

The x-axis of the trend chart represents time. The time span of the axis can be set with a fixed start and end time or with an end time relative to the present time. The axis can be quick-scaled to show the last hour, last day, last month, or last year​.

 
action_zoom_plus_stroke Absolute time span and relative time span, schematic
图: Absolute time span and relative time span, schematic

The y-axis refers to the measurement unit that the variable represents. The scale of the y-axis can be set manually or by auto scale. You can configure the trend chart to present series on one y-axis or two y-axes, one to the left and one to the right. Use two y-axes to present series with different ranges in the same trend chart.

 
action_zoom_plus_stroke One y-axis and two y-axes, schematic
图: One y-axis and two y-axes, schematic

To make reading easier, grid lines can be shown in the trend chart. Grid lines can be shown in both the x- and y-direction, independent of each other.

 
action_zoom_plus_stroke Grid lines, schematic
图: Grid lines, schematic
  • Trend Charts
  • Trends Overview
  • Configuring a Trend Chart
  • Editing the Trend Chart Settings
  • Configuring the X-Axis with a Relative Time Span
  • Configuring the X-Axis with an Absolute Time Span
  • Automatically Configuring the Y-Axis Scale
  • Scrolling the Trend Chart X-Axis to the Current Time
  • Showing Trend Chart Grid Lines
  • Assigning a Series to a Y-Axis
  • Trend Chart Settings Dialog Box – Axes Tab
  • Trend Chart View