earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Automation Server, AS-B, Enterprise Central, Enterprise Server, AS-P, WorkStation, Virtual Project Servers
Functionalities: Trends
Product version: 2.0, 2.1, 3.0, 3.1
11/26/2018

Trend Chart Event Icons

Use the Trend Chart event icons to get information on different trend log events.

Table: Trend chart event icons

Icon

Description

 
action_zoom_plus_stroke

Log was started

Indicates that the trend log started recording values.

 
action_zoom_plus_stroke

Log was stopped

Indicates that the trend log stopped recording values.

 
action_zoom_plus_stroke

The log is not configured

Indicates that the trend log is not correctly configured or preferences are missing, so the trend log cannot start recording values.

 
action_zoom_plus_stroke

A log value was missed

Indicates that one or more records were missed due to interrupted communication, hardware failure, or software failure.

 
action_zoom_plus_stroke

The log configuration was updated

Indicates that the settings of the trend log were updated. The change is described in the ToolTip of the event.

 
action_zoom_plus_stroke

Record was added

Indicates that a record was manually added. The new value is described in the event ToolTip.

 
action_zoom_plus_stroke

Record was edited

Indicates that a record was manually edited. The change is described in the ToolTip of the event.

 
action_zoom_plus_stroke

Record was added and commented

Indicates that a record was manually added and commented. The new value and comment are described in the ToolTip of the event.

 
action_zoom_plus_stroke

Record was edited and commented

Indicates that a record was manually edited and commented. The changes are described in the ToolTip of the event.

 
action_zoom_plus_stroke

Record was commented

Indicates that a record was commented. The comment is shown in the ToolTip of the event.

 
action_zoom_plus_stroke

Log was cleared

Indicates that a trend log was cleared.

 
action_zoom_plus_stroke

Meter was changed

Indicates that the meter was changed or that the settings were configured. This icon only applies to the meter trend log.

 
action_zoom_plus_stroke

Values exist outside the viewable area

Indicates that values exist before the values displayed in the trend chart area.

 
action_zoom_plus_stroke

Values exist outside the viewable area

Indicates that values exist after the values displayed in the trend chart area.

 
action_zoom_plus_stroke

INF value was logged

Indicates that a positive Infinity value was logged.

 
action_zoom_plus_stroke

-INF value was logged

Indicates that a negative Infinity value was logged.

 
action_zoom_plus_stroke

NaN value was logged

Indicates that an unknown value ("Not a Number") was logged.

 
action_zoom_plus_stroke

Null value was logged

Indicates that a Null value was logged.

 
action_zoom_plus_stroke

System clock changed

Indicates that the system date and time of the EcoStruxure BMS server where the trend log is located has been changed. For more information, see Time and Time Zone .

 
action_zoom_plus_stroke

Override

Indicates that the recorded value is overridden by the hardware and is not the measured value. For more information, see Output Override Status .

Forced

Indicates that the recorded value is forced by the software and is not the measured value. For more information, see Forced I/O Point Values .

 
action_zoom_plus_stroke

Log database restored

Indicates that the log database has been restored and that, when the log restarts, there can be a time gap in the log series.

 
action_zoom_plus_stroke

Log reset by extended log

Indicates that the log has been cleared by the extended trend log due to a log database restore.

 
action_zoom_plus_stroke

Transfer was missed

Indicates that the extended trend log has miss records between fetches. That is, the monitored log has created and lost records before the extended trend log has been able to fetch the records.

  • Trend Charts
  • Real-Time Plotting
  • Temporary Trend Log Lists
  • Series Tab Context Menu
  • Trend Log Does Not Start Record Due to the Start Condition
  • Missing Trend Log Records
  • Trend Chart Does Not Show Trend Log Series
  • Interrupted Series in the Trend Chart
  • Trend Chart Live Update does not Work
  • Trend Chart Y-Axis has Scale Problems
  • Trend Chart View