earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface de utilizador

Interface de utilizador


Produtos: AS-B, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Funcionalidades: Tendências
Versão do produto: 3.2, 3.3, 2022
15-10-2020

Trend Chart Navigation Bar

Use the Trend Chart navigation bar to horizontally scroll the trend chart.

Tabela: Trend Chart Navigation Bar

Component

Description

 
action_zoom_plus_stroke

Log start

Click to scroll back to the first value of the trend chart in WorkStation.

 
action_zoom_plus_stroke

Fast backward

Click to scroll fast backward.

 
action_zoom_plus_stroke

Backward

Click to scroll back.

Live update

Select to have the trend chart automatically adjust itself according to the latest trend log record in WorkStation.

 
action_zoom_plus_stroke

Forward

Click to scroll forward.

 
action_zoom_plus_stroke

Fast forward

Click to scroll fast forward.

 
action_zoom_plus_stroke

Current time

Click to scroll forward to the latest value of the trend chart in WorkStation.

  • Trend Charts
  • Trend Chart View