earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Trends
Product version: 3.2, 3.3, 2022
7/13/2021

Trend Chart Series Properties

Use the Trend Chart Series Properties dialog box to configure the properties of the trend chart series.

 
action_zoom_plus_stroke Trend chart series properties
Figure: Trend chart series properties

Table: Trend Chart Series Properties

Component

Description

Display trend log

Displays the path the trend log series is connected to.

Y- axis

Select Left to attach the series to the left y-axis.

Series presentation

Select the presentation of the series: line, discrete line, binary, or bars.

Color

Enter the color of the series.

Weight

Enter the weight of the line. The line-weight value is a value without correlation to any unit of measure.

Show markers

Select True to show a marker for each record. The marker can only be shown for lines and discrete lines, not for digital and bars.

Show events

Select True to show event symbols in the trend chart.

Calculation method

Select the calculation method to calculate the recorded values before displaying the series in the trend chart.

Delta over period

Select True to apply a period to the delta calculation method.

Period

Select the time span for which the calculation method is to be executed.

Custom period

Enter a custom time span for which the calculation method is to be executed

Custom period alignment

Enter the time when you want the custom period to start.

  • Trend Charts
  • Trend Chart Properties
  • Trend Series
  • General Information Properties – Basic Tab
  • References Tab