earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: Enterprise Central, Enterprise Server, Project Configuration Tool
功能: 基本功能
产品版本: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2021/7/13

Trend Log Archive File

Use the Trend Log Archive to view the history of a trend log.

 
action_zoom_plus_stroke Trend log archive file
图: Trend log archive file

表格: Trend Log Archive File

Column

Description

TYPE

​Displays the object type that defines the properties of the object.

SEQNO

Displays the trend or event sequence number.

TimeStamp

Displays the date and time when a record or event was generated.

RefSeqNo

Displays a reference to another record by sequence number, used by edits and comments.

OriginalSeqNo

Displays the original sequence number from the original log stored by the extended trend log.

User

Displays the user that generated the event.

Comment

Displays the comment that was added to a record when it was edited.

Event

Displays if something is missing or something unexpected happens. 有关更多信息,请参阅 Trend Log Enumerations .

EndTime

​​Displays the time when the old meter was replaced.

EndValue

​Displays the value the old meter had when it was replaced.

StartTime

​Displays the time when the new meter was installed.

StartValue

​Displays the value of the new meter when it was installed.

MeterConstant

​Displays the constant of the new meter. If the meter counts in kilo (10 3 ), the constant is 1000.

MinValue

​Displays the first value of the new meter after roll-over.

MaxValue

​Displays the last value of the new meter before roll-over.

Value

Displays the value of a record.

EditTime

Displays the time of the record that is added manually to a manual trend log.

LogType

The type of the trend log that has been edited.

Description

Displays the trend log property that has been configured.

Status

Displays the status of the trend log. 有关更多信息,请参阅 Trend Log Enumerations .

  • Trend Log Enumerations
  • Archiving Overview
  • Archive Folders, Files, and Names
  • Manually Creating an Archive
  • Creating a Scheduled Archive
  • Archive Log Contents