earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: WebReports
功能: 报告
产品版本: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
2021/12/16

Trend Log Comparison Report

The Trend Log Comparison report provides a way for you to compare the output of the trend logs associated with a data point, such as the kilowatts for a power meter. The report provides similar reporting as the Trend Chart, however, you can export the report, schedule the report, and run the report using a Web browser and without access to WorkStation.

The following table shows the input parameters for the report.

表格: Trend Log Comparison Input Parameters

Input Parameters

Description

Start report date/time

Specifies the start date and time for tracking all trend log data points.

End report date/time

Specifies the end date and time for tracking all trend log data points.

Date filter

Specifies the date range of an operation, such as an alarm trigger, the running of a report schedule, or a read by the Reporting Agent.

For example, if you select Last 7 days for an alarm report, the report displays information about all alarms that were triggered during the last 7 days. If you select Last 7 days for the Report schedule report, the report displays information about all Report schedules that were run during the last 7 days. If you select Last 7 days for the Reporting Agent report, the report displays information about all Reporting Agent reads that occurred during the last 7 days.

Select Fixed date if you entered a Start report date/time and an End report date/time .

Ext. trend logs

Specifies the extended trend logs that you want to compare.

Report view

Specifies the format, such as a table, for displaying the report.

  • Factory Supplied Reports
  • Production Reports
  • WebReports Submit Form Page