earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Tendencias
Versión del producto: 2.0, 2.1, 3.0, 3.1
18/05/2018

Trend Log Functions

arrow1_rotationLog Record Storage arrow1_rotationTrend Log Activation arrow1_rotationExtended Trend Logs

​All trend logs store records by using the circular storing principle; you can also connect trends logs to external trend logs with larger storing capacity. For some trend logs you can set up conditions that have to be fulfilled before the trend log starts recording.

Log Record Storage

​All trend logs use circular storing. How many records a trend log can store before overwriting old ones depends on the trend log configuration.

Para obtener más información, consulte Almacenamiento de entradas en el registro .

Trend Log Activation

​The interval trend log and change of value trend log start recording values when the configured activation conditions are met. If an activation variable is used, both the activation variable and the activation time have to be true for the trend log to start recording.

Para obtener más información, consulte Trend Log Activation .

Extended Trend Logs

​You use an extended trend log to transfer records from a trend log. An extended trend log can be connected to a trend log or connected in a series to another extended trend log. Only one extended trend log can be connected to a trend log.

Para obtener más información, consulte Registros de tendencias ampliados .

  • Trends Overview
  • Almacenamiento de entradas en el registro
  • Trend Log Activation
  • Registros de tendencias ampliados
  • Viewing Related Trends
  • Viewing Related Trends for Properties Bound to a Graphic