earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-L, AS-B, Enterprise Server, AS-P, Project Configuration Tool
功能: 趋势
产品版本: 1.9
2017/10/12

Trend Log Functions

arrow1_rotationLog Record Storage arrow1_rotationTrend Log Activation arrow1_rotationExtended Trend Logs

​All trend logs store records by using the circular storing principle; you can also connect trends logs to external trend logs with larger storing capacity. For some trend logs you can set up conditions that have to be fulfilled before the trend log starts recording.

Log Record Storage

​All trend logs use circular storing. How many records a trend log can store before overwriting old ones depends on the trend log configuration.

有关更多信息,请参阅 日志记录存储 .

Trend Log Activation

​The interval trend log and change of value trend log start recording values when the configured activation conditions are met. If an activation variable is used, both the activation variable and the activation time have to be true for the trend log to start recording.

有关更多信息,请参阅 Trend Log Activation .

Extended Trend Logs

​You use an extended trend log to transfer records from a trend log. An extended trend log can be connected to a trend log or connected in a series to another extended trend log. Only one extended trend log can be connected to a trend log.

有关更多信息,请参阅 扩展趋势日志 .

  • Trends Overview
  • 日志记录存储
  • Trend Log Activation
  • 扩展趋势日志
  • Viewing Related Trends
  • Viewing Related Trends for Properties Bound to a Graphic