earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 趋势
产品版本: 2.0, 2.1, 3.0, 3.1
2018/12/20

Trend Log List – Log Info View

When expanded, the Log Info view displays a summary of the data recorded in the trend log list.

注释:
  • The log info does not include records that are not displayed in the trend log list. The log info data changes with the trend log when the trend log list is refreshed or reopened.

 
action_zoom_plus_stroke Log info view
图: Log info view

表格: Log Info View

Component

Description

Log name

The name of the log that is connected to the trend log list.

Log unit

The unit of the recorded values.

Calculation method

The calculation method connected to the trend log list, if any.

Start time

The time of the first record in the trend log list.

Highest value

The highest value in the trend log list.

Average

The average value of the trend log list.

Displayed trend log

The trend log that is connected to the trend log list.

Stop time

The time of the last record in the trend log list.

Lowest value

The lowest value in the trend log list.

Number of records

The number of records to be stored before old records are overwritten.

  • Trend Log Lists
  • Time Zone Modes in a Trend Log List
  • Trend Log List View
  • Trend Log List Properties