earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Tendencias
Versión del producto: 2.0, 2.1, 3.0, 3.1
20/12/2018

Trend Log List Event Icons

Use the trend log list event icons to get information on different trend log events.

Tabla: Trend Log List Event Icons

Icon

Description

 
action_zoom_plus_stroke

Log was started

Indicates that the trend log started recording values.

 
action_zoom_plus_stroke

Log was stopped

Indicates that the trend log stopped recording values.

 
action_zoom_plus_stroke

The log is not configured

Indicates that the trend log is not correctly configured or preferences are missing, so the trend log cannot start recording values.

 
action_zoom_plus_stroke

A log value was missed

Indicates that one or more records were missed due to interrupted communication, hardware failure, or software failure.

 
action_zoom_plus_stroke

The log configuration was updated

Indicates that the settings of the trend log were updated. The change is described in the comment column of the table.

 
action_zoom_plus_stroke

Record was added

Indicates that a record was manually added.

 
action_zoom_plus_stroke

Record was edited

Indicates that a record was manually edited.

 
action_zoom_plus_stroke

Record was commented

Indicates that a log record was commented. The comment is displayed in the ToolTip of the event and in the comment column of the table.

 
action_zoom_plus_stroke

Log was cleared

Indicates that a trend log was cleared.

 
action_zoom_plus_stroke

Meter was changed

Indicates that the meter was changed or that the settings were configured.

This event symbol only applies to the meter trend log.

 
action_zoom_plus_stroke

System clock changed

Indicates that the system date or time, where the trend log is located, has been changed. Para obtener más información, consulte Time and Time Zone .

 
action_zoom_plus_stroke

Override

Indicates that the recorded value is overridden by the hardware and is not the measured value. Para obtener más información, consulte Output Override Status .

Forced

Indicates that the recorded value is forced by the software and is not the measured value. Para obtener más información, consulte Forced I/O Point Values .

 
action_zoom_plus_stroke

Log database restored

Indicates that the log database has been restored and that, when the log restarts, there can be a time gap in the log series.​

 
action_zoom_plus_stroke

Log reset by extended log

Indicates that the commands from the extended trend log have been cleared from the trend log.

  • Trend Log Lists
  • Time and Time Zone
  • Time Zone Modes in a Trend Log List
  • Interrupted Series in the Trend Chart
  • Illogical or Missing Records in the Trend Log List
  • Trend Log List View