earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 趋势
产品版本: 2023
2022/12/17

Trend Log List Properties

Use the Trend Log List properties to configure the trend log list.

 
action_zoom_plus_stroke Trend log list properties
图: Trend log list properties

表格: Trend Log List Properties

Component

Description

Display trend log

Enter the trend log to display in the trend log list.

Log space (records)

​Select the maximum number of records to display in the trend log list.

Show events

Select True to display events in the trend log list. This function does not hide events in the list that contain a value or comment. For example, when a record is added, edited, or commented.

Time zone

Select which time perspective to display in the trend log. 有关更多信息,请参阅 Time Zone Modes in a Trend Log List .

Calculation method

Select a calculation method.

Delta over period

Select True to apply a period to the delta calculation method.

Period

Select the time span for which the calculation method is to be executed.

Custom period

Enter a custom time span for which the calculation method is to be executed.

Custom period alignment

Enter the time when you want the custom period to start.

  • Trend Log Lists
  • Time Zone Modes in a Trend Log List
  • Trend Log List Context Menu
  • Trend Log List Toolbar
  • Trend Log List – Log Info View
  • General Information Properties – Basic Tab
  • References Tab