Use the Configure Interval Trend Log page to configure the settings of the interval trend log.
Component |
Description |
Logged variable |
Enter the variable that you want to log. |
|
Set unit Click to open the Unit Selection dialog box where you select the unit. Pour plus d'informations, voir Select Unit Dialog Box . |
Delta |
Select the minimum value change that triggers a new record. |
Activation variable |
Enter the variable that is to make the trend log start recording values when the variable is true. |
Activation time |
Specify the time when the trend log is to start recording values. |
Interval |
Type how often to log the variable, the interval defines the time between two log records. |
Log size |
Select the number of records to store before old records are overwritten including internal records generated by the trend. |
Available trend storage |
Displays the trend storage usage and the number of records left in the trend storage. |
Clear when enabled |
Select True to clear the trend log when it is enabled. |