earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Server, Project Configuration Tool
功能: 趋势
产品版本: 1.8
2016/10/13

Create Trend Log Wizard – Configure Interval Trend Log Page

Use the Configure Interval Trend Log page to configure the settings of the interval trend log.

 
action_zoom_plus_stroke Configure Interval Trend Log page
图: Configure Interval Trend Log page

表格: Configure Interval Trend Log Page

Component

Description

Logged variable

Enter the variable that you want to log.

 
action_zoom_plus_stroke

Set unit

Click to open the Unit Selection dialog box where you select the unit. 有关更多信息,请参阅 Unit Selection Dialog Box .

Delta

​Select the minimum value change that triggers a new record.

Activation variable

Enter the variable that is to make the trend log start recording values when the variable is true.

Activation time

Specify the time when the trend log is to start recording values.

Interval

Type how often to log the variable, the interval defines the time between two log records.

Log size

Select the number of records to store before old records are overwritten including internal records generated by the trend.

Available trend storage

Displays the trend storage usage and the number of records left in the trend storage.

Clear when enabled

​Select True to clear the trend log when it is enabled.

  • Interval Trend Logs
  • Interval Trend Log Properties
  • Unit Selection Dialog Box
  • Trend Units
  • Interval Trend Log Delta
  • Trend Log Activation
  • Log Record Storage
  • Create Object Wizard – Naming the Object Page