earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Trends
Product version: 2024, 7.0
12/3/2024

Create Manual Trend Log Wizard – Configure Manual Log Page

Use the Configure Manual Log page to configure the settings of a manual log.

 
action_zoom_plus_stroke Configure manual log page
Figure: Configure manual log page

Table: Configure Manual Log Page

Component

Description

Unit

Enter the unit of the records in the trend log list. For more information, see Trend Units .

  • Manual Trend Logs
  • Manual Trend Log Properties – Basic Tab
  • Create Object Dialog – Naming the Object Page