Use the Configure Meter Trend Log page to configure the settings of the meter trend log.
Component |
Description |
Logged variable |
Enter the variable that you want to log. |
![]() |
Set unit Click to open the Unit Selection dialog box where you select the unit. For more information, see Unit Selection Dialog Box . |
Trigger variable |
Enter the variable that triggers the trend log to start recording. |
Trigger condition |
Select when you want the variable recorded: when trigger variable changes to true, changes to false, or all changes. For more information, see Variable Triggered Trend Logs . |
Log size |
Select the number of records to store before old records are overwritten including internal records generated by the trend. |
Available trend storage |
Displays the trend storage usage and the number of records left in the trend storage. |
Clear when enabled |
Select True to clear the trend log when it is enabled. |