earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Automation Server, AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Trends
Product version: 2.0, 2.1, 3.0, 3.1
10/24/2018

Create Trend Chart Wizard – Configure Trend Chart Page

Use the Configure Trend Chart page to configure the settings of the trend chart.

 
action_zoom_plus_stroke Configure trend chart page
Figure: Configure trend chart page

Table: Configure Trend Chart Page

Component

Description

Time mode

​Select the time mode of the x-axis.

Start time

Enter the absolute start time when Time mode is set to Absolute. This time is the leftmost point of the x-axis.

Stop time

Enter the absolute stop time when Time mode is set to Absolute . This time is the rightmost point of the x-axis.

Time span

When time mode is set to Relative the leftmost x-axis value is equal current time minus Time span . Where the rightmost x-axis value is current time.

Auto scale left Y-axis

Select to activate auto scale. The scale of the left Y-axis adapts itself to the displayed series.

Series

Displays all series in the trend chart.

 
action_zoom_plus_stroke

Add

Click to add a series to the trend chart. For more information, see Create Object Wizard – Naming the Object Page .

 
action_zoom_plus_stroke

Edit

Click to edit a selected series. For more information, see Trend Chart Series Properties .

 
action_zoom_plus_stroke

Remove

​Click to remove a selected series.

  • Trend Charts
  • Create Object Wizard – Naming the Object Page
  • Trend Chart Properties