Use the Configure Trend Chart page to configure the settings of the trend chart.
Component |
Description |
Time mode |
Select the time mode of the x-axis. |
Start time |
Enter the absolute start time when Time mode is set to Absolute. This time is the leftmost point of the x-axis. |
Stop time |
Enter the absolute stop time when Time mode is set to Absolute . This time is the rightmost point of the x-axis. |
Time span |
When time mode is set to Relative the leftmost x-axis value is equal current time minus Time span . Where the rightmost x-axis value is current time. |
Auto scale left Y-axis |
Select to activate auto scale. The scale of the left Y-axis adapts itself to the displayed series. |
Series |
Displays all series in the trend chart. |
|
Add Click to add a series to the trend chart. Więcej informacji zawiera Create Object Dialog – Naming the Object Page . |
|
Edit Click to edit a selected series. Więcej informacji zawiera Trend Chart Series Properties . |
|
Remove Click to remove a selected series. |