earth_america
user_standard 登录
action_search_stroke
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 趋势
产品版本: 2024, 7.0
2024/12/3

Create Trend Chart Wizard – Configure Trend Chart Page

Use the Configure Trend Chart page to configure the settings of the trend chart.

 
action_zoom_plus_stroke Configure trend chart page
图: Configure trend chart page

表格: Configure Trend Chart Page

Component

Description

Component

Description

Time mode

​Select the time mode of the x-axis.

Start time

Enter the absolute start time when Time mode is set to Absolute. This time is the leftmost point of the x-axis.

Stop time

Enter the absolute stop time when Time mode is set to Absolute . This time is the rightmost point of the x-axis.

Time span

When time mode is set to Relative the leftmost x-axis value is equal current time minus Time span . Where the rightmost x-axis value is current time.

Auto scale left Y-axis

Select to activate auto scale. The scale of the left Y-axis adapts itself to the displayed series.

Series

Displays all series in the trend chart.

 
action_zoom_plus_stroke

Add

Click to add a series to the trend chart. 有关更多信息,请参阅 Create Object Dialog – Naming the Object Page .

 
action_zoom_plus_stroke

Edit

Click to edit a selected series. 有关更多信息,请参阅 Trend Chart Series Properties .

 
action_zoom_plus_stroke

Remove

​Click to remove a selected series.

  • Trend Charts
  • Create Object Dialog – Naming the Object Page
  • Trend Chart Properties