earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface de utilizador

Interface de utilizador


Produtos: AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Tendências
Versão do produto: 3.2, 3.3, 2022
15-10-2020

Create Trend Log List Wizard – Configure Trend Log List Page

Use the Configure Trend Log List page to create a trend log list that presents the records from a trend log.

 
action_zoom_plus_stroke Configure trend log list page
Imagem: Configure trend log list page

Tabela: Configure Trend Log List Page

Component

Description

Display trend log

Enter the trend log you want to present in the trend log list.

Log space (records)

​Select the maximum number of records to display in the list.

  • Trend Log Lists
  • Trend Log List Properties
  • Create Object Dialog – Naming the Object Page