earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Пользовательский интерфейс

Пользовательский интерфейс


Продукты: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Функции: Тренды
Версия продукта: 2024, 7.0
03.12.2024

Create Trend Chart Wizard – Configure Trend Log Series Page

Use the Configure Trend Log Series page to add a series to the trend chart or multiple trend log list that presents a trend log.

 
action_zoom_plus_stroke Configure trend log series page
Рисунок: Configure trend log series page

Таблица: Configure Trend Log Series Page

Component

Description

Display trend log

Enter the trend log you want to present as a series in the trend chart.

Weight

Type the weight of the line. The value has no correlation to any unit of measure.

Show markers

Select True to show a marker for each record. The marker can only be shown for lines and discrete lines, not for digital and bars.

Show events

Select True to show event symbols in the trend chart.

  • Trend Charts
  • Trend Chart Settings Dialog Box – Series Tab