earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Tendencias
Versión del producto: 2.0, 2.1, 3.0, 3.1
25/10/2018

Create Trend Log Wizard – Connect Objects to the Trend Log Page

Use the Connect Objects to the Trend Log page to connect the trend log to an extended trend log, trend log list, or trend chart.

 
action_zoom_plus_stroke Connect objects to the trend log page
Figura: Connect objects to the trend log page

Tabla: Connect Objects to the Trend Log Page

Component

Description

Extended Trend Log

Click the browse button to start the wizard to create an extended trend log and connect it to the trend log.

Trend Log List

Click the browse button to start the wizard to create a trend log list and connect it to the trend log.

Trend Chart

Click the browse button to start the wizard to connect the trend log to a new trend or a existing trend chart.

  • Registros de tendencias ampliados
  • Trend Log Lists
  • Gráficos de tendencias