Funkcje: Trendy
Wersja produktu: 3.2, 3.3, 2022
2020-10-15

Create Trend Log Wizard – Connect Objects to the Trend Log Page

Use the Connect Objects to the Trend Log page to connect the trend log to an extended trend log, trend log list, or trend chart.

 
action_zoom_plus_stroke Connect objects to the trend log page
Rysunek: Connect objects to the trend log page

Tabela: Connect Objects to the Trend Log Page

Component

Description

Extended Trend Log

Click the browse button to start the wizard to create an extended trend log and connect it to the trend log.

Trend Log List

Click the browse button to start the wizard to create a trend log list and connect it to the trend log.

Trend Chart

Click the browse button to start the wizard to connect the trend log to a new trend or a existing trend chart.

  • Extended Trend Logs
  • Trend Log Lists
  • Trend Charts