earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Пользовательский интерфейс

Пользовательский интерфейс


Продукты: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Функции: Тренды
Версия продукта: 2024, 7.0
03.12.2024

Create Trend Log Wizard – Connect Objects to the Trend Log Page

Use the Connect Objects to the Trend Log page to connect the trend log to an extended trend log, trend log list, or trend chart.

 
action_zoom_plus_stroke Connect objects to the trend log page
Рисунок: Connect objects to the trend log page

Таблица: Connect Objects to the Trend Log Page

Component

Description

Extended Trend Log

Click the browse button to start the wizard to create an extended trend log and connect it to the trend log.

Trend Log List

Click the browse button to start the wizard to create a trend log list and connect it to the trend log.

Trend Chart

Click the browse button to start the wizard to connect the trend log to a new trend or a existing trend chart.

  • Extended Trend Logs
  • Trend Log Lists
  • Trend Charts