earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-L, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Tendencias
Versión del producto: 1.9
12/10/2017

Actions Menu – Activation Submenu

Use the Activation submenu to enable, disable, or clear a trend log.

 
action_zoom_plus_stroke The trend log Actions menu, Activation submenu
Figura: The trend log Actions menu, Activation submenu

Tabla: Activation Submenu

Command

Description

Enable trend log

Click to enable the trend log. The trend log starts when the start condition is fulfilled.

Disable trend log

Click to disable the trend log and stop all recording activity.

Clear trend log

Click to clear all the records from the trend log.

Force transfer

Click to manually forces the transfer of records to the extended trend log.

  • Registros de tendencias ampliados
  • Actions Menu