earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 趋势
产品版本: 2024, 7.0
2024/12/2

Actions Menu – Activation Submenu

Use the Activation submenu to enable, disable, or clear a trend log.

 
action_zoom_plus_stroke The trend log Actions menu, Activation submenu
图: The trend log Actions menu, Activation submenu

表格: Activation Submenu

Command

Description

Enable trend log

Click to enable the trend log. The trend log starts when the start condition is fulfilled.

Disable trend log

Click to disable the trend log and stop all recording activity.

Clear trend log

Click to clear all the records from the trend log.

Force transfer

Click to manually forces the transfer of records to the extended trend log.

  • Extended Trend Logs
  • Actions Menu